המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is included in the PME 7.2.2 starter kit (IE7BYNCZZSPEZZ)
Issue
User wants to know what is included in the PME starter kit activation license

Product
Power Monitoring Expert (PME) 7.2.2

Environment
PME licensing

Resolution
The following licensed components are included with the activation:
-Base Power Monitoring Expert 7.2 software license
-1 x Engineering Client  license
-2 x Web Client licenses
-1 x DL-S high-end device license
-9 x DL-E entry-level device licenses

If additional device licenses are required, the PME Starter Kit is fully expandable using standard PME part numbers.