המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What profile should be used in PSE to add a PM5560

Language:
English

Issue:
In Profile Editor, there are two PM5000 options: PM5000S and PM5000S1.

Product Line:

• Power SCADA Operations 8.2

• Power Operation 2020

• Power Operation 2021

• Power Operation 2022

• Power Operation 2023

• Power Operation 2024

Environment:
Profile Editor

Resolution:
Select the PM5000S profile to add a PM5560 device to a project.

Recommendation:

If you are using an older version of

Power Operation, consider upgrading to the latest version for improved protocol support and security. For assistance with integration or upgrades, contact Schneider Electric Technical Support at: pmo-psup@se.com

Support details