המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
TLC calculation in single phase testing mode

Issue
User would like to know how the Transformer Loss Compensation is calculated in Single phase testing mode of ION 7550/7650 or ION8600/8650

Product line
ION7550

ION7650

ION8600

ION8650

Environment

TLC Calculations

Cause

Understanding the calculations will allow users to follow Transformer Loss Compensation measurements while testing is enabled.

Resolution
Single-phase test option lets you use a single-phase source and view three phase. When the single-phase testing is enabled, the meter will calculate the V2 Average, V4 Average and I2 average from the single-phase source according to the following calculations:

For a Wye system:

TLC Measurement for a wye system in an ION Meter
For a Delta system:

TLC Measurement for a delta system in an ION Meter

The above parameters are then used to calculate the losses according to the following:
TLC Measurement using both delta and wye system in an ION Meter
You can also connect a single‐phase source voltage input in parallel and the current in series to simulate a three‐phase source without toggling to the single-phase mode.