המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can a standalone StruxureWare Power Monitoring Expert 7.2.2 system be moved from a Standalone Server to a Distributed system?
Issue
Migrating from a PME 7.2.2 Standalone System to a PME 7.2.2 Distributed System

Product Line
Power Monitoring 7.2.2

Environment
Standalone System to Distributed System

Cause
It is sometimes desirable to migrate from standalone architecture to distributed system while keeping the data, configuration and setup intact.

Resolution

*Warning: This article contains information about editing the registry. Improper changes to the registry can permanently damage the operating system. Always backup the registry before making any changes.*

*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

See the attached document for instructions on how to Migrate from a standalone to distributed system architecture.

שניידר אלקטריק ישראל

קבצים מצורפים
PME_7.2.2standalonetodistributed.pdf [151.7 KB]
גלה עוד
מוצר:
גלה עוד
מוצר: