המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is "+/- Speed Around Reference" on the ATV61 or ATV71 drive?
Issue:
Using "+/- Speed Around a Reference" on the ATV61 or ATV71 drive.

Product Line:
ATV61, ATV71

Environment:
All models and serial numbers

Cause:
NA

Resolution:
+/- Speed Around a Reference is a way to adjust the motor speed above or below a given Speed reference. One application for Speed Around Reference is to run a secondary conveyor belt above or below the speed  of a primary conveyor belt with a single speed reference going to both drives. It may be a case where two conveyor belts are feeding a single conveyor.  The single conveyor may need to run at a slightly higher speed to keep product moving.  See the ATV61 or ATV71 programming manual for details.