המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What can cause an OC3 fault on the ATV21 and ATV212 drives?
Issue:
Why does OC3 trips on the ATV21/ATV212 drives?

Product Line:
Altivar ATV21 ATV212 S-Flex

Environment:
All models

Cause:
The drive is running and intermittently trips on the OC3 fault.

Resolution:
OC3 means overcurrent during constant speed operation.

Possible causes:
Abrupt fluctuations in the load or abnormal load conditions.

Remedies:
Reduce the load fluctuations
Check your load
Set parameter F316 to 1 or 3

OC3 can be cleared by Auto Restart as long as the condition that causes the fault is resolved.
To turn on Auto Restart set F303 to any value between 1 and 10. This value is the number attempts to clear the fault.