המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Trying to control or start the ATV61 drive using Somove the error message "The command is already active in another channel " comes up.
Issue:
Getting the message The Command is Already Active in Another Channel when trying to control the ATV61 or ATV71 in SoMove

Product Line:
Altivar ATV61 ATV71 with SoMove

Environment:
All

Cause:
Trying to control or start the drive using Somove the error message "The command is already active in another channel " comes up.

Resolution:
Check your Command status to see if HMI is the reference or command.  On the ATV61 Drive check the F4 function key to see if you are in LOC or REM mode.  If you are in LOC mode you will need to put the drive in REM mode before you can control it over Somove.

vfvv

nhy