המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the differences between Com’X 510 & EGX300?
The differences between Com'X 510 & EGX300
. Com'X 510: Real time trending not yet available
. Com'X 510: Custom Web Page support not yet available
. Com'X 510: Not compliant with all device types found in EGX300
. * Com'X 510: Improved choices for dashboard comparison
. * Com'X 510: Improved data capacity.(32 devices, 30 topics each at 15 minute intervals = 25 months of data)
. * Com'X 510: Wire less connection availability (WiFi and GPRS for external communication, Zigbee Module not yet available )
. * Com'X 510: Onboard  six digital and two analog  inputs
. * Com'X 510: Data publication availability to Digital Server Platform (DSP) with just one menu choice
. * Com'X 510: Secure ability to publish data via a CSV file using HTTP(S)
* designates improvement over EGX300