המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How can I configure an M580 PAC to log events to a syslog Server?
Goals and Symptoms
Syslog is a standard messaging service that can be used to monitor security and other events. It is available on the M580 using
Unity Pro version 10.0 or greater. The attached document  is a descriptive example of using syslog with Unity.

Facts and Changes
In a system using syslog the M580 acts as a client sending messages to a syslog server. Each message is time-stamped
and an NTP or SNTP server must also be configured. This example uses a BME P58 1020 PAC. The NTP server is a
TCSESM083F2CU0 Connexium switch. The syslog server is an open source server Visual Syslog. The configuration of each is
described in the attachment.

שניידר אלקטריק ישראל

קבצים מצורפים
SYSLOG .pdf [1.09 MB]