המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to derive a default IP address from a MAC address of a Unity Momentum processor.

Issue:

How to derive a default IP address from a MAC address of a Unity Momentum processor.

Product:

Unity Momentum

Resolution:

The processor derives its default IP address from its factory-assigned MAC address. The MAC address for the processor is displayed on the front of the module. The default address is in the format 10.10.x.y, where x and y are derived from the last 2 octets of the MAC address. To determine the default IP address of a module, follow these steps..
IP Address calculation
NOTE: There are many resources for converting hex numbers to decimal numbers. For example,
you can use the Windows calculator in scientific mode.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)