המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do you change the default display setting on an ATV12 drive?
Issue:
ATV212 default display adjustment

Product line:
ATV12, Altivar 12

Environment:
All

Cause:
n/a

Resolution:
The default display for the ATV12 will show Output Frequency.  To change this, enter into the Monitor menu (NOn).  Select the desired value you would like to see.  Push Enter a second time on that value and it will save your setting.

Some common options are:
rFr - Output Frequency
Frh - Reference Frequency
ULn - Line voltage
LCr - motor current

For further options, please consult the User Manual, document number BBV28581