המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the ambient temperature operating range of the ATV12 series drives?

Article available in these languages: Spanish

Issue:
ATV12 ambient temperature operating range

Product Line:
ATV12 series drives.

Environment:
All models, All serial numbers.

Cause:
N/A

Resolution:

Ambient Air Temperature**

ATV12H018F1, ATV12H037F1
ATV12H018M2...H075M2
ATV12H018M3...H075M3
ATV12P models
Operation -10C to +40C without derating.  Up to +60C with derating.  Remove the blanking cover and de-rate at 2% per degree above 40C.

ATV12H075F1
ATV12HU15M2, HU22M2
ATV12HU15M3...HU40M3
Operation -10C to +50C without derating.  Up to +60C with derating.  Remove the blanking cover and de-rate at 2% per degree above 50C.

Storage temperature for all units is -25C to +70C

** UL ratings are up to 40C only.  Higher temperature ratings listed above are for non-UL listed applications only.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)