המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the efficiency rating for the ATV212 series drives?
Issue:
ATV212 efficiency rating.

Product Line:
ATV212 series drives.

Environment:
All models, as listed in the attached documents.

Cause:
Information available in current literature is too generic, customer requires more specific information.

Resolution:
For efficiency of the ATV212 it can be calculated for 100% by using the formula :

(Pn - Loss) / Pn.

Pn : nominal Power.
See Loss: in the file attachment