המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
BMXART0814 appears to be consuming two additional registers.
Issue
BMXART0814 appears to be consuming two additional registers.

Product Line
BMXART0814

Environment
Unity, Control Expert

Resolution
If you configure a BMXART0814 and an analog module (e.g., BMXAMI0810) with no gap in the state ram assignment between the
two modules, the first two registers of the analog will appear not to work or overwritten.

The reason this occurs is because the BMXART0814 reserves two additional registers for the cold junction.

The workaround is to allocate a two register gap between the two modules.