איך נוכל לעזור לך היום?

how to avoid restoring all factory setting of the ATV32 behind a during the Boot-up?

Some STB Network Interface Module sends during the Boot-up the SDO parameter (1011:01) to restore all manufacturing parameters.
As the Boot-up can't be setting in STB NIM, we can avoid this if needed by setting the ATV32.
To reject the SDO parameter (1011:01) the bit7 of the Application Hidden Word AP01 have to be activated.
see pdf for the "how to activate the bit 7".

שניידר אלקטריק ישראל

קבצים מצורפים
How to activate the bit7.pdf [351.84 KB]