המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why is the subscription report says successful when sent to the printer but nothing prints?
Issue
Unable to print subscription reports from PME/Web Applications/Reports even when it says it was successful.
If the report is saved to the desktop, it prints OK.
From the Desktop works because it is using Windows not PME.

Product Line
All versions of Power Monitoring Expert (PME)

Environment
Power Monitoring Expert
Printing Reports


Cause
The installed printer does not allow printing from subscription reports in PME/Web Applications/Reports.

Resolution
In order to print pdf subscription reports, a TRUE PDF printer needs to be installed.
The printer specifications needs to include PDF under the  Page Description Languages as shown below.


Page Description Languages (PDL)
PCL® 5c, PCL® 6, PDF direct, PostScript 3 compatible

שניידר אלקטריק ישראל

גלה עוד
מוצר:
גלה עוד
מוצר: