המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Migrating from E-Series to Q-Series Trio Data Radios

As of Trio Q-Series firmware version 1.36, the Q-Series radios are now able to use an E/M Emulation mode to talk to an existing E and/or M Series radios.

While operating in E Emulation mode, the Trio Q and the Trio E have the following similarities:
• RF and bit error rate performance
• General functionality and operation
• User configurable features and options
• Local and remote diagnostics and network management capability

Full details of functional differences, hardware changes and programming requirements can be found in the Product Migration Guide. Please contact your local distributor for more information about the Q-Series data radios.

שניידר אלקטריק ישראל

קבצים מצורפים
Trio E to Trio Q Product Migration Guide.pdf [1.51 MB]