המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
VIP13 relay - is there a replacement for the legacy VIP13 protection relay?
Please see the files attached to this FAQ for more information.

The VIP13 has been discontinued in 2004 and can be replaced by the VIP300P, which is still available through Schneider distribution centers.

The 2 products use the same current sensors: CSa for 630A and CSb for 1250A.

The cases have different form factors so an adaptation kit is needed. This kit, designed by Ecofit activity, is not available anymore.  However it's a simple plate so it should not be difficult for a system integrator also attached a view of VIP300P front panel and all the info I found on VIP13 / 300P.  Note: the VIP range is designed by AED based on an MVS specification and it is sold by MVS (not AED, except for spare parts)

שניידר אלקטריק ישראל

קבצים מצורפים
Case_21539154_VIP13_VIP300_DMO.zip [1.16 MB]