המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video on how to flash the firmware in a M221 controller.

Issue:
How to upgrade firmware in a M221 controller using the Machine Expert Basic (formally SoMachine Basic) software.

Product Line:
Machine Expert Basic formally SoMachine Basic and all M221 controllers.

Envionment:
Machine Expert Basic SoMachine Basic

Cause:
Not able to perform new functions that were added into the software and firmware.

Resolution:
This is a video on the steps to follow to flash the firmware into the M221 controller.  The firmware is included in this software version package.