המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Do all Unity Pro/Control Expert packages support the LL984 language?
Unity Pro SUnity Pro LUnity Pro XLUnity Pro XLS
Function Block Diagram FBD++++
Ladder Diagram (LD) language++++
Instruction List IL++++(2)
Structured Text ST++++(2)
Sequential Language SFC++++(2)
Ladder Logic 984 (LL984)++++
Libraries (1)
Standard library++++(2)
Control library++++(2)
Communication library++++(2)
Diagnostics library++++(2)
I/O management library++++(2)
System library++++(2)
Motion control drive library-+++(2)
TCP Open library-optionaloptionaloptional (2)
Obsolete library++++(2)
MFB library++++(2)
Safety library---+
Memory card file management library++++(2)
Create and use data structures (DDTs)++++(2)
Create and use Derived Function Blocks (DFBs)++++
Project browser with structural and/or functional view++++
Managing access rights++++
Operator screen++++
Diagnostic viewer++++
System diagnostics++++
Project diagnostics++++(2)
Trending Tool++++
Application converterPL7 converter Concept Converter Partial conversionPL7 converter Concept ConverterPL7 converter Concept ConverterPL7 converter Concept Converter
Modicon M340BMX P34 1000 BMX P34 20••BMX P34 1000 BMX P34 20••BMX P34 1000 BMX P34 20••BMX P34 1000 BMX P34 20••
Modicon M580-BME P58 1020
BME P58 2020
BME P58 3020
All CPUs-
Momentum171CBU78090
171CBU98090
171CBU98091
171CBU78090 171CBU98090 171CBU98091171CBU78090
171CBU98090
171CBU98091
171CBU78090
171CBU98090
171CBU98091
Premium-All CPUs except: P57 554M P57 5634M P57 6634MAll CPUsAll CPUs
Quantum-140 CPU 311 10
140 CPU 434 12 U/A* 140 CPU 534 14 U/A* * Upgrade using Unity OS
CPU 311 10 CPU 434 12 U/A CPU 534 14 U/A CPU 651 50 CPU 651 60 CPU 652 60 CPU 658 60 CPU 670 60 CPU 671 60 CPU 672 60 CPU 672 61 CPU 678 61CPU 311 10 CPU 434 12 U/A CPU 534 14 U/A CPU 651 50 CPU 651 60 CPU 652 60 CPU 658 60 CPU 670 60 CPU 671 60 CPU 672 60 CPU 672 61 CPU 678 61 CPU 651 60S CPU 671 60S
Atrium-All CPUsAll CPUsAll CPUs
Simulator++++
Hyperlinks++++
Documentation as context help and PDF++++
OS Loader tool + HW firmware++++
Unity Loader++++

+ (1)   Availability of the blocks depends on the hardware platforms (see Unity Pro, Standard, Block Library).
+ (2)  Available on all PLC except platforms CPU 651 60S, CPU 671 60S. - = not available