המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to upgrade firmware on a BCPM series meters
Product Line
BCPM
DLF-3000

Environment
Firmware Upgrade

Resolution
*Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance.*

*Warning: Devices should be disconnected from all monitoring software before performing a firmware upgrade*


BCPM series meters firmware can be upgraded using DLF-3000 by following the attached procedure. Firmware v1.023 is attached to this article as well.

Use the following link to download the DLF-3000 software:
DLF3000 Download

שניידר אלקטריק ישראל

קבצים מצורפים
BCPM upgrade procedure.pdf [659.19 KB]