המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to determine which method to use for importing a third party manufacture eds file, if the hardware type is not known.
Issue
How to determine which method to use for importing a third party manufacture eds file, if the hardware type is not known.

Product Line
Unity

Environment
Windows 10

Resolution
The quickest way to determine which method to use for importing the eds file is view the '.eds' file with Notepad.

fdsf


If the device is described as an EthernetIP hardware the 'Add EDS to Library' selection in the DTM Browser must
be used to import the eds file.
  • Right click on the DTM hostname.
  • Click on 'Device menu'.
  • Click on 'Additional functions.
  • Click on 'Add EDS to library.
serfrf
  • Click on 'Next'.
wefr
  • Click on 'Add files'.
  • Click on 'Browse' and locate the edds file.
  • Click on 'Next'.
fewf


The 'DTM Catalog 'Update' button accessed from within Unity must be used. to update the hardware catalog.
  • Click on 'Tools\Hardare Catalog' to open the 'Hardware Catalog' window.
  • Click on 'DTM Catalog'.
  • Click on 'Update'.
wfrf


If the device is not described, it is most likely a CANOpen type hardware. The 'Hardware Catalog Manager'
must be used to import he eds file.
erf