המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Are there any system variables in Vijeo Designer to extract the Time of Day (TOD) clock from a Magelis/Harmony HMI?
Issue:
Are there any system variables in Vijeo Designer to extract the Time of Day (TOD) clock from a Magelis/Harmony HMI?

Product Line:
All Vijeo Designer HMIs

Environment:
TOD clock, system clock

Resolution:
Vijeo Designer does indeed have system variables for the TOD clock.
Below is a list of the system variables available:
_Hour
_Minutes
_Seconds
_Month
_Day
_DayoftheWeek (Sunday = 1, Monday =2, ...,  Saturday = 7)
_Year2 (last two digits of the current year)
_Year4 (all 4 digits of the current year

The data type of all of these values is "DINT".