המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Does the ATV630 Process drive have embedded Ethernet TCP/IP and Ethernet IP?

Article available in these languages: Spanish

The ATV600 series drives have an embedded Ethernet port that supports Modbus TCP/IP and a Modbus RTU port.
For Ethernet IP an option card must be installed.
Either VW3A3720 or VW3A3721
Option card Instruction Bulletin is available here: https://www.se.com/us/en/download/document/EAV64328/

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)