המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to disable COM port on ION8650

Issue
Disabling COM port on ION8650 is desired so no communication can be done through that COM port for security reasons.

Product Line
ION8650A
ION8650B
ION8650C

Environment
ION Setup 3.0
ION8650 Communication port

Resolution
1) Upgrade firmware version for ION8650 meter to the latest firmware version (Currently V4.40)

2)In ION Setup, in Setup Assistant, navigate to Communications -> Serial Settings. Choose the COM port tab that needs to be disabled. Change the protocol for that COM port to "None."

ION Setup Assistant


Changing the protocol can also be achieved fromthe front display of the meter. Go to ION8650 SETUP by holding "ALT/ENTER" button. Navigate to the COM port that needs to be disabled. Click "Enter" on PROTOCOL and change it to "NONE"