איך נוכל לעזור לך היום?

How to set up properly the time out parameters to succeed the NOR communication between Server & Client

Question:
How to set up properly the time out parameters to succeed the NOR communication between Server & Client. In Specific, what's relationship of timeout, offline poll period and link status period between server & client to assure its smooth communication.


Answer:
In general, the relationship of  LinkStatusPeriod, Max retries and Offline Poll Period is as below and keep same  Offline Poll Period for client and server.

Server: Confirm Timeout* Max retries < Client: Offline Poll Period
Client: Confirm Timeout* Max retries < Server: Offline Poll Period

Confirm Timeout< LinkStatusPeriod < Offline Poll Period