המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do you send an ASCII string out from a Schneider (Modicon) M340 or M580 with ModbusTCP/IP?

Product Line:
M340, M580, X80

Environment:
Ecostruxure Control Expert

Resolution:
Unfortunately, you cannot;
The M340 and M580 ethernet ports can only send or receive Modbus TCP/IP or Ethernet/IP messaging. They cannot read or write in ASCII characters using these protocols.
The only option is to use the M340 Modbus serial port or BMX NOM 0200 module with the INPUT_CHAR or the PRINT_CHAR function blocks to read and write an ASCII string to or from a server device.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)