המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do I reset the kWh value stored in my ATV21 or ATV212 drive?

Issue:
Wants to reset the accumulated kWh in the ATV21 or ATV212 drive.

Product Line:
Altivar 21 or Altivar 212
S-Flex

Environment:
All part numbers, all models

Cause:
kWh needs to be reset

Resolution:
To reset the kWh in the drive, change F748 to 0 and then cycle power.

Changing it to 0 tells the drive not to save the setting to EEPROM.
Cycling power will clear the currently saved value and reset it back to 0.

Then you can turn F748 back to 1 so it will retain the kWh until the next time you want to reset it.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)