המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the part number for the remote keypad for the ATV32 variable speed drive?
Issue:
Part number for the remote keypad of ATV32 drive.

Product Line:
ATV32

Environment:
All

Cause:
Product Selection

Resolution:
​There are three keypad options for the ATV32 drives.

Option 1
VW3A1101 is an LCD keypad display.
VW3A1102 is the remote mounting kit with bezel providing IP54 rating.
VW3A1103 is an optional clear door providing IP65 rating and tamper resistance.
A cable is offered in several lengths:
VW3A1104R10 for a 1 meter cable.
VW3A1104R30 for a 3 meter cable.
VW3A1104R50 for a 5 meter cable.
VW3A1104R100 for a 10 meter cable.

Option 2:
VW3A1006 is a 4 digit LED keypad display rated IP54.
Use a cable from option 1 above.

Option 3
VW3A1007 is a 4 digit LED keypad display rated IP65.
Use a cable from option 1 above.