המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How does the ATV630 Process drives stall function work?

Article available in these languages: Spanish

Issue:
How to set up stall function on the ATV630 Process drive?

Product Line:
Altivar 630

Environment:
All serial numbers

Cause:
Stall function

Resolution:
This function helps to prevent a motor overload by monitoring the motor current and the speed rise time.
A stalling condition is when:
An output frequency is smaller than the stalling frequency [Stall Frequency] StP3
And an output current is higher than the stalling current [Stall Current] StP2
During a time longer than the stalling time [Stall Max Time] StP1
That means that you must meet three conditions, then a stalling condition occurs, an [Motor Stall Error] StF error is triggered.

For example,
Set StP3=10HZ, StP2=100% (meaning rated motor current)
StP1=5s
When the drive is running at 9.9HZ, motor current is above rated motor current, then after 5S, an [Motor Stall Error] StF error is triggered.
If the drive is running at 10.1HZ, an StF error is not triggered.