המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What are the difference between TIME and LTIME data types in Machine Expert?
TIME is a 32 bit data type. The resolution is in milliseconds.

LTIME is a 64 bit data type. The resolution in nanoseconds.


Example of variable declarations:

var_0 AT %MD0: TIME;    // %MD0 overlaps with %MW0 and %MW1
var_1 AT %MD1: TIME;    // %MD1 overlaps with %MW2 and %MW3

var_2 AT %ML0: LTIME;   // %ML0 overlaps with %MW0, %MW1, %MW2 and %MW3
var_3 AT %ML1: LTIME;   // %ML1 overlaps with %MW4, %MW5, %MW6 and %MW7