המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is it possible to capture current values of %MW , %M and un-located variables ?
Yes. In fact there are two ways to do it.

1: Using the Data Editor declare Initial Values for the variables and turn on the "Save" attribute in Data Properties (This will require a build changes).
Unity will now be able to update Initial values with Current values when online. This action will overwrite the Data Editor's Initial Values

2: Create a DTX file by using the option "Save Data from PLC to File". The data stored in the DTX file can be downloaded
to the PLC by using the "Restore Data from File to PLC".