המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why is "transfer license to USB device" grayed out in Vijeo Designer's License Manager?

Issue:
Unable to transfer the Vijeo Designer license to a USB / Removable Media device when Computer ID is unknown. The option is no longer available in the License Manager.

Product Line:
Vijeo Designer (all versions)

Resolution:
This feature is purposely grayed out as we do not support transfer to USB device for Vijeo Designer's license. We prefer a more secure option of transferring to removable media only when the destination computer ID is known. This method prevents unauthorized PCs from taking the license and prevents the risk of losing the license.

With Vijeo Designer V6.2 it is possible to transfer the license via a removable media.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)