המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is PME vulnerable to the GNU glibc CVE-2015-7547

Issue

User wants to know if Power Monitoring Expert (PME) is vulnerable to the exploit described in GNU glibc CVE-2015-7547.

Product Line

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

PME Supported Operating Systems

Cause

The vulnerability CVE-2015-7547 affects systems using the GNU glibc library, which is part of Linux-based environments. PME runs on Windows operating systems, which do not use glibc. Therefore, PME is not impacted by this exploit.

Resolution

PME is not vulnerable to this exploit.