המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do you configure an R-Function key in Vijeo Designer for an XBTGK/HMIGK?
Issue:
It is not clear how we configure the R-Function Keys on an XBTGK/HMIGK in Vijeo Designer. Where is the configuration done?

Product Line:
Vijeo Designer V6.2, XBTGK, HMIGK

Resolution:
In order to configure an R-Function Key in Vijeo Designer, you must first click on the panel you wish to configure the key for. In the property inspector for the panel, you will see a property called "Function Key".

Open the configuration dialog and you will see the configurable settings for the key.