המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video: How to create a HMISCU project in SoMachine 4.1 and download it to an USB stick

Issue:
How to create a HMISCU project in SoMachine 4.1 and download it to an USB stick

Product Line:
HMISCU

Environment:
SoMachine 4.1 SP2

Resolution:

The following video FAQ will show how to create a HMISCU project in SoMachine 4.1 and download it to an USB stick



If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)