המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to program force fire control on the ATV212/21?
Issue:
Set up the force fire control on the ATV212/21.

Product Line:
Altivar 21, Altivar 212

Environment:
All serial numbers

Cause:
VFD programming for forced fire control

Resolution:
WARNING
LOSS OF CONTROL
The value of F650 will impact the direction of the motor.
- Check wiring motor power UVW is correct.
- Verify that the value of F650 is convenient for this application.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

To program the VFD for Forced Fire control, program the following parameters:
F650 –  Forced fire control
0 - Disable
1 - Enable Forward
2 - Enable Reverse
-Note: Parameter F311 must be set to allow the motor direction set by F650
Once F650 is set press and hold the enter key for 2 seconds

F294 – Forced speed frequency when drive is in the forced mode

F111, F112 or F113 – Must be set to 53, this would be the assignment of a logic input to Fire/Forced mode.