המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Will Vijeo Designer Runtime 6.2 run on Windows 10?
Issue:
Looking to confirm if Vijeo Designer Runtime 6.2 will run on Windows 10

Product Line:
Vijeo Designer V6.2

Resolution:
As of Vijeo Designer 6.2 SP6, all tests have been completed to certify that Vijeo Designer Runtime can run on Windows 10. When installing Vijeo Designer V6.2 (base version), ensure you right-click on the install.exe file and "Run As Administrator". This will ensure you have full privileges to install the software. Once you have installed the base version, apply any service pack SP6 or greater.