איך נוכל לעזור לך היום?

Does the Power Monitoring Expert Installer Support Silent Mode or Command Line Installs

Issue
Customer would like to use scripts to automate the install of PME or SPM engineering clients

Product

Struxureware Power Monitoring 7.0(SPM)

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024



Environment
Installer

Resolution
The Installer does not support silent mode or command line argument installs