המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
My SoMachine controller stops in exception for no obvious reason and I have some function blocks declared as retain
In Somachine v4.x it is not possible to declare function blocks as retain as this can cause exceptions.
But it is still possible to declare variables as retain inside function blocks.

Declaring function blocks as retain is possible with Machine Expert.
(Note that retain variables consume less memory than full function blocks).