המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Clicking on the Settings link on the Power Monitoring Expert main page pops up an error window

Issue
When I use clicks on the "Settings" link on the Power Monitoring Expert main page a new error window pops up with link to GeneralSettingsDialog.html not found

Product
Power Monitoring Expert 8.1

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment
Main web site is using non default address like /PQweb instead of the default /web

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).*

1) Navigate to [PME install]\Applications\ApplicationFramework\content
2) Backup the file GeneralSettingsDialog.js
3) Edit the original file with a text editor
Replace the line TemplateUtil.LocAndLoad('/Web/Content/GeneralSettingsDialog.html', with the correct with the setup URL
For example
TemplateUtil.LocAndLoad('/PQWeb/Content/GeneralSettingsDialog.html',
4) Close all web clients and restart IIS
5) Verify that the link now opens the settings page.