המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
IP camera tested with HMIG5U

Following references have been tested with success on HMIG5U on Internet explorer (by using Internet Explorer Browser in tool chest or IE11 directly) for both video flow and camera control:
- Pelco SPECTRA 4 IP
- D-Link cloud ptz camera dcs-5222L

Additional Information:
- Tests have been done with VJD6.2 SP4 with HMIG5U+DT651.
- Both Internet Explorer 11 and Vijeo Designer Run Time can show camera contents and control is allowed only after install cab files.
- For Pelco camera, the cab files have been installed from camera drivers provided in the camera box.
- For D-Link camera, the cab files have been downloaded form Dlinl Web site.