המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the diagnostic step in Config ELEC ?
With the diagnostic, you can check the consistency between the information seen by the product and what you can see in the electrical switchboard.
So you can test that the parameters you filled in during the configuration and product connections are ok for a full functional system.
The diagnostic is recommended by Schneider Electric to check that your system is working well once configured.