המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where can I get documentation on Short Circuit Current Ratings on the Altivar 900 drives?
Issue:
Short Circuit Current Ratings documentation for the Altivar 900.

Product Line:
ATV900

Environment:
All serial numbers for ATV900

Cause:
Need to get information on fuses and circuit breaker ratings

Resolution:
Please reference the attached document NHA61583
https://www.se.com/ww/en/download/document/NHA61583/​

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)