המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to autoload the Recipes from a RecipeSelect object in Vijeo Designer?
Issue:
Is it possible to autoload Recipes in Vijeo Designer?

Product Line:
Vijeo Designer (all versions)

Resolution:
It is possible to program a recipe to autoload in Vijeo Designer. In the RecipeSelect object properties, there is an option called AutoLoadRecipe. If set to TRUE, the recipe ingredient values will load automatically when the recipe name is selected at runtime.
recipe auto select