המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the voltage supply to the ATS48 fan kits?

Issue:
Voltage supply to the ATS48 fan kits.

Product line:
ATS48, Altistart 48

Cause:
OHF - Overheating

Resolution:
The cooling fans are supplied with 12Vdc.  The voltage tolerance on the fans is 6-13Vdc, 315mA.  You can test operation of the fans with something such as a 9V battery, if a 12Vdc source is not available.  This should provide enough power to move the fans.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)