המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to View the Members of an Active Directory Group

Issue
How to view the members of an Active Directory group if you aren't a domain admin and cannot log into to a domain controller.

Product

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Environment
Windows Active Directory

Cause
While troubleshooting a suspected permission or configuration issue, it may be necessary to view and verify the members of a Windows Active Directory group
in order to determine that a particular user has been granted the correct access rights.

Resolution
From a computer that is a member of the domain, open a command-prompt and run the following command replacing <group name> with the
name of the group you are interested in.

NET GROUP "<group name>" /DOMAIN

Unless the permissions on the group object have been changed from the default security settings and set to restrict from viewing, the group memberships are visible using this method.
You will not be permitted to change any group membership settings.

שניידר אלקטריק ישראל

גלה עוד
מוצר:
גלה עוד
מוצר: