המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to View the Details of a Active Directory User Account

Issue
How to display the detailed information of an Active Directory User's account.

Product

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024


Environment
Windows Active Directory

Cause
While troubleshooting an suspected permissions or configuration issue, it may be necessary to view and verify a particular Active Directory User's account information in order to determine there are no issues with the account and/or the account has been configured with appropriate parameters.  (i.e. the password has not expired or recently been changed and the User has been included in the appropriate groups)

Resolution
From a computer that is a member of the domain, open a command-prompt and run the following command replacing <user name> with the name
of the user you are interested in.

NET USER "<user name>" /DOMAIN

This same command can retrieve the local computer user account information as well by removing the /DOMAIN parameterand providing the name of a local user's account.

שניידר אלקטריק ישראל

גלה עוד
מוצר:
גלה עוד
מוצר: