איך נוכל לעזור לך היום?

How can I compare two strings in SoMachine v4.1 SP2?

To compare two strings data type in SoMachine you can use the EQ function block.

The input pins of the EQ can be any data type including string.
If the string values are equal the output is true, if different the output is false.
EQ function block