המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What steps need to be taken to determine the ROOT cause of an EC02 / EC0E / EC0x error on a Quantum CPU?


We'll need several items to forward to R&D which will be used to determine root cause of failure.

1: Please provide a copy of the application file in STA format (Archive Project).
2: What version of Unity or Control Expert are you using?
3: What is the S/N and PV level of the CPU? This info is visible in the LED window below
the display.
4: What version of CPU firmware, and what version of Copro firmware is being used?
You can use the Keypad and select System Info / Firmware .
5: After power cycling the PLC connect to the processor and
Select Help\About Unity Pro XL
Select Technical Support
Browse To a folder where the Diagnostic file will be stored
Select OK

Unity will generate a DIAG file and an Log file and place them into the folder declared above.
Send these files and the information described above to us .